public static class FlangeBuilder.LengthTypeOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INSIDE_DIMENSION
The flange length is dimensioned to the Inner Mold line.
|
static int |
_OUTSIDE_DIMENSION
The flange length is dimensioned to the Outer Mold Line.
|
static int |
_WEB_DIMENSION
The flange length is dimensioned to the Bend Tangent Line.
|
static FlangeBuilder.LengthTypeOptions |
INSIDE_DIMENSION
The flange length is dimensioned to the Inner Mold line.
|
static FlangeBuilder.LengthTypeOptions |
OUTSIDE_DIMENSION
The flange length is dimensioned to the Outer Mold Line.
|
static FlangeBuilder.LengthTypeOptions |
WEB_DIMENSION
The flange length is dimensioned to the Bend Tangent Line.
|
Modifier and Type | Method and Description |
---|---|
static FlangeBuilder.LengthTypeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.LengthTypeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.LengthTypeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final FlangeBuilder.LengthTypeOptions INSIDE_DIMENSION
public static final FlangeBuilder.LengthTypeOptions OUTSIDE_DIMENSION
public static final FlangeBuilder.LengthTypeOptions WEB_DIMENSION
public static final int _INSIDE_DIMENSION
public static final int _OUTSIDE_DIMENSION
public static final int _WEB_DIMENSION
public static FlangeBuilder.LengthTypeOptions valueOf(int value)
public static FlangeBuilder.LengthTypeOptions valueOf(String name)
public static FlangeBuilder.LengthTypeOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.