public static class DimpleBuilder.SidewallTypeOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INSIDE
the outerface of the dimple side walls coincides with the section outline.
|
static int |
_OUTSIDE
the innerface of the dimple side walls coincides with the section outline.
|
static DimpleBuilder.SidewallTypeOptions |
INSIDE
the outerface of the dimple side walls coincides with the section outline.
|
static DimpleBuilder.SidewallTypeOptions |
OUTSIDE
the innerface of the dimple side walls coincides with the section outline.
|
Modifier and Type | Method and Description |
---|---|
static DimpleBuilder.SidewallTypeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DimpleBuilder.SidewallTypeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DimpleBuilder.SidewallTypeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final DimpleBuilder.SidewallTypeOptions OUTSIDE
public static final DimpleBuilder.SidewallTypeOptions INSIDE
public static final int _OUTSIDE
public static final int _INSIDE
public static DimpleBuilder.SidewallTypeOptions valueOf(int value)
public static DimpleBuilder.SidewallTypeOptions valueOf(String name)
public static DimpleBuilder.SidewallTypeOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.