public static class TrimCurveBuilder.SecondBoundingObjectEndOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
Trim second bounding object from end
|
static int |
_START
Trim second ounding object from start
|
static TrimCurveBuilder.SecondBoundingObjectEndOptions |
END
Trim second bounding object from end
|
static TrimCurveBuilder.SecondBoundingObjectEndOptions |
START
Trim second ounding object from start
|
Modifier and Type | Method and Description |
---|---|
static TrimCurveBuilder.SecondBoundingObjectEndOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.SecondBoundingObjectEndOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.SecondBoundingObjectEndOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final TrimCurveBuilder.SecondBoundingObjectEndOptions START
public static final TrimCurveBuilder.SecondBoundingObjectEndOptions END
public static final int _START
public static final int _END
public static TrimCurveBuilder.SecondBoundingObjectEndOptions valueOf(int value)
public static TrimCurveBuilder.SecondBoundingObjectEndOptions valueOf(String name)
public static TrimCurveBuilder.SecondBoundingObjectEndOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.