public static class TrimCurveBuilder.FirstBoundingObjectEndOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
Trim first bounding object from end
|
static int |
_START
Trim first bounding object from start
|
static TrimCurveBuilder.FirstBoundingObjectEndOptions |
END
Trim first bounding object from end
|
static TrimCurveBuilder.FirstBoundingObjectEndOptions |
START
Trim first bounding object from start
|
Modifier and Type | Method and Description |
---|---|
static TrimCurveBuilder.FirstBoundingObjectEndOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.FirstBoundingObjectEndOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.FirstBoundingObjectEndOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final TrimCurveBuilder.FirstBoundingObjectEndOptions START
public static final TrimCurveBuilder.FirstBoundingObjectEndOptions END
public static final int _START
public static final int _END
public static TrimCurveBuilder.FirstBoundingObjectEndOptions valueOf(int value)
public static TrimCurveBuilder.FirstBoundingObjectEndOptions valueOf(String name)
public static TrimCurveBuilder.FirstBoundingObjectEndOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.