public static class ReplaceFaceBuilder.ReplaceTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_REPLACE
This stands for replace type - to replace the surface of the target face with the tool face
|
static int |
_SIMPLIFY
This stands for simplify type - to simplify the geometry representation of a surface of a face
|
static ReplaceFaceBuilder.ReplaceTypes |
REPLACE
This stands for replace type - to replace the surface of the target face with the tool face
|
static ReplaceFaceBuilder.ReplaceTypes |
SIMPLIFY
This stands for simplify type - to simplify the geometry representation of a surface of a face
|
Modifier and Type | Method and Description |
---|---|
static ReplaceFaceBuilder.ReplaceTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReplaceFaceBuilder.ReplaceTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReplaceFaceBuilder.ReplaceTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ReplaceFaceBuilder.ReplaceTypes REPLACE
public static final ReplaceFaceBuilder.ReplaceTypes SIMPLIFY
public static final int _REPLACE
public static final int _SIMPLIFY
public static ReplaceFaceBuilder.ReplaceTypes valueOf(int value)
public static ReplaceFaceBuilder.ReplaceTypes valueOf(String name)
public static ReplaceFaceBuilder.ReplaceTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.