Modifier and Type | Interface and Description |
---|---|
static class |
RasterImage.MaxTextureSize
Specifies the maximum number of pixels to allow for the width or height
of a raster image.
|
Feature.BooleanType, Feature.DiagnosticType
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
double |
height()
Returns the height of the image, given in part units (mm or in)
License requirements: None. |
String |
imageFileName()
Returns the name of the image file used for the raster image.
|
double |
length()
Returns the length of the image, given in part units (mm or in).
|
Matrix3x3 |
matrix()
Returns the rotation matrix of the raster image
License requirements: None. |
RasterImage.MaxTextureSize |
maximumTextureSize()
Returns the enum value for the maximum size of the image, in pixels
License requirements: None. |
Point3d |
origin()
Returns the origin of the raster image
License requirements: None. |
double |
translucency()
Returns the translucency of the raster image, in range [0.0, 1.0]
License requirements: None. |
void |
update(Point3d origin,
Matrix3x3 matrix,
double length,
double height,
String imageFileName,
double translucency,
RasterImage.MaxTextureSize maximumTextureSize)
Updates a raster image feature
License requirements: studio_visualize ("STUDIO VISUALIZE") . |
algorithmVersion, breakWaveLink, changeBooleanType, containerFeature, deleteClueAlerts, deleteHintAlerts, deleteInformationalAlerts, deleteWarningAlerts, featureType, getAllChildren, getChildren, getEntities, getExpressions, getFeatureClueHintMessages, getFeatureClueMessages, getFeatureColor, getFeatureErrorMessages, getFeatureHintMessages, getFeatureInformationalMessages, getFeatureName, getFeatureWarningMessages, getParents, getSections, hideBody, hideParents, highlight, isContainedFeature, isInternal, location, logDiagnostic, makeCurrentFeature, makeSketchExternal, makeSketchInternal, removeForEdit, removeParameters, setGroupActive, showBody, showDimensions, showParents, suppress, suppressed, timestamp, unhighlight, unsuppress
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getPdmReferenceAttributeValue, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setPdmReferenceAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
Point3d origin() throws NXException, RemoteException
NXException
RemoteException
Matrix3x3 matrix() throws NXException, RemoteException
NXException
RemoteException
double length() throws NXException, RemoteException
NXException
RemoteException
double height() throws NXException, RemoteException
NXException
RemoteException
String imageFileName() throws NXException, RemoteException
NXException
RemoteException
double translucency() throws NXException, RemoteException
NXException
RemoteException
RasterImage.MaxTextureSize maximumTextureSize() throws NXException, RemoteException
NXException
RemoteException
void update(Point3d origin, Matrix3x3 matrix, double length, double height, String imageFileName, double translucency, RasterImage.MaxTextureSize maximumTextureSize) throws NXException, RemoteException
origin
- The origin for the raster imagematrix
- The rotation matrix for the raster imagelength
- Length of the image, given in part units (mm or in)height
- Height of the image, give in part units (mm or in)imageFileName
- Name of the image file to use.
For now, it must be a .tif filetranslucency
- 0.0 for no translucency, 1.0 for fully tranparentmaximumTextureSize
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.