public static class ExtractFaceBuilder.FaceSurfaceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_GENERAL_BSURFACE
extracted surface is a B-surface approximation of the original surface
|
static int |
_POLYNOMIAL_CUBIC
extracted surface is a cubic polynomial approximation of the original surface
|
static int |
_SAME_AS_ORIGINAL
extracted surface is the same as the original surface
|
static ExtractFaceBuilder.FaceSurfaceType |
GENERAL_BSURFACE
extracted surface is a B-surface approximation of the original surface
|
static ExtractFaceBuilder.FaceSurfaceType |
POLYNOMIAL_CUBIC
extracted surface is a cubic polynomial approximation of the original surface
|
static ExtractFaceBuilder.FaceSurfaceType |
SAME_AS_ORIGINAL
extracted surface is the same as the original surface
|
Modifier and Type | Method and Description |
---|---|
static ExtractFaceBuilder.FaceSurfaceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtractFaceBuilder.FaceSurfaceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtractFaceBuilder.FaceSurfaceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExtractFaceBuilder.FaceSurfaceType SAME_AS_ORIGINAL
public static final ExtractFaceBuilder.FaceSurfaceType POLYNOMIAL_CUBIC
public static final ExtractFaceBuilder.FaceSurfaceType GENERAL_BSURFACE
public static final int _SAME_AS_ORIGINAL
public static final int _POLYNOMIAL_CUBIC
public static final int _GENERAL_BSURFACE
public static ExtractFaceBuilder.FaceSurfaceType valueOf(int value)
public static ExtractFaceBuilder.FaceSurfaceType valueOf(String name)
public static ExtractFaceBuilder.FaceSurfaceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.