public static class DivideCurveBuilder.InputArcLengthDirectionFlag extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
Input Arc length from end
|
static int |
_START
Input Arc length from start
|
static DivideCurveBuilder.InputArcLengthDirectionFlag |
END
Input Arc length from end
|
static DivideCurveBuilder.InputArcLengthDirectionFlag |
START
Input Arc length from start
|
Modifier and Type | Method and Description |
---|---|
static DivideCurveBuilder.InputArcLengthDirectionFlag |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DivideCurveBuilder.InputArcLengthDirectionFlag |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DivideCurveBuilder.InputArcLengthDirectionFlag[] |
values()
Returns an array that contains the values for this enum.
|
public static final DivideCurveBuilder.InputArcLengthDirectionFlag START
public static final DivideCurveBuilder.InputArcLengthDirectionFlag END
public static final int _START
public static final int _END
public static DivideCurveBuilder.InputArcLengthDirectionFlag valueOf(int value)
public static DivideCurveBuilder.InputArcLengthDirectionFlag valueOf(String name)
public static DivideCurveBuilder.InputArcLengthDirectionFlag[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.