public interface CutFaceBuilder extends FeatureBuilder
FeatureCollection.createCutFaceBuilder(nxopen.features.Feature)
Property | Value |
---|---|
FaceToCut.CoaxialEnabled | 0 |
FaceToCut.CoplanarAxesEnabled | 0 |
FaceToCut.CoplanarEnabled | 0 |
FaceToCut.EqualDiameterEnabled | 0 |
FaceToCut.OffsetEnabled | 0 |
FaceToCut.ParallelEnabled | 0 |
FaceToCut.PerpendicularEnabled | 0 |
FaceToCut.SymmetricEnabled | 0 |
FaceToCut.TangentEnabled | 0 |
FaceToCut.ThicknessChainEnabled | 0 |
FaceToCut.UseFaceBrowse | 1 |
Motion.DeltaEnum | ReferenceWcsWorkPart |
Motion.DeltaXc.Value | 0.0 |
Motion.DeltaYc.Value | 0.0 |
Motion.DeltaZc.Value | 0.0 |
Motion.Option | DistanceAngle |
Modifier and Type | Method and Description |
---|---|
boolean |
doPaste()
Returns the do paste option defines whether paste the cut faces to a target body.
|
FaceRecognitionBuilder |
faceToCut()
Returns the face recognition builder holding the faces to cut.
|
ModlMotion |
motion()
Returns the motion about which the cut faces move
License requirements: None. |
boolean |
reverseDirection()
Returns the reverse direction.
|
void |
setDoPaste(boolean doPaste)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setReverseDirection(boolean reverseDirection)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
SelectBody |
targetBody()
Returns the target body.
|
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
FaceRecognitionBuilder faceToCut() throws NXException, RemoteException
NXException
RemoteException
ModlMotion motion() throws NXException, RemoteException
NXException
RemoteException
boolean doPaste() throws NXException, RemoteException
NXException
RemoteException
void setDoPaste(boolean doPaste) throws NXException, RemoteException
doPaste
- NXException
RemoteException
SelectBody targetBody() throws NXException, RemoteException
NXException
RemoteException
boolean reverseDirection() throws NXException, RemoteException
NXException
RemoteException
void setReverseDirection(boolean reverseDirection) throws NXException, RemoteException
reverseDirection
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.