public static class BodyByEquationBuilder.LocationTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EMBEDDED
Worksheet is embedded in part.
|
static int |
_OPERATING_SYSTEM
Worksheet is on the native OS file system.
|
static int |
_TEAMCENTER
Worksheet is in Teamcenter.
|
static BodyByEquationBuilder.LocationTypes |
EMBEDDED
Worksheet is embedded in part.
|
static BodyByEquationBuilder.LocationTypes |
OPERATING_SYSTEM
Worksheet is on the native OS file system.
|
static BodyByEquationBuilder.LocationTypes |
TEAMCENTER
Worksheet is in Teamcenter.
|
Modifier and Type | Method and Description |
---|---|
static BodyByEquationBuilder.LocationTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BodyByEquationBuilder.LocationTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BodyByEquationBuilder.LocationTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final BodyByEquationBuilder.LocationTypes OPERATING_SYSTEM
public static final BodyByEquationBuilder.LocationTypes TEAMCENTER
public static final BodyByEquationBuilder.LocationTypes EMBEDDED
public static final int _OPERATING_SYSTEM
public static final int _TEAMCENTER
public static final int _EMBEDDED
public static BodyByEquationBuilder.LocationTypes valueOf(int value)
public static BodyByEquationBuilder.LocationTypes valueOf(String name)
public static BodyByEquationBuilder.LocationTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.