public static class SubdivideFacetBodyBuilder.InterpolationMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CUBIC
In the cubic option the sub-triangles are fitted cubic to the surrounding triangles.
|
static int |
_LINEAR
In the linear option the sub-triangles are coplanar to the original triangle.
|
static SubdivideFacetBodyBuilder.InterpolationMethodType |
CUBIC
In the cubic option the sub-triangles are fitted cubic to the surrounding triangles.
|
static SubdivideFacetBodyBuilder.InterpolationMethodType |
LINEAR
In the linear option the sub-triangles are coplanar to the original triangle.
|
Modifier and Type | Method and Description |
---|---|
static SubdivideFacetBodyBuilder.InterpolationMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivideFacetBodyBuilder.InterpolationMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivideFacetBodyBuilder.InterpolationMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SubdivideFacetBodyBuilder.InterpolationMethodType LINEAR
public static final SubdivideFacetBodyBuilder.InterpolationMethodType CUBIC
public static final int _LINEAR
public static final int _CUBIC
public static SubdivideFacetBodyBuilder.InterpolationMethodType valueOf(int value)
public static SubdivideFacetBodyBuilder.InterpolationMethodType valueOf(String name)
public static SubdivideFacetBodyBuilder.InterpolationMethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.