public static class DecimateFacetBodyBuilder.DecimateMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CHORDAL_DEVIATION
Chordal deviation reduces the number of facets by removing facets which do not effect the overall accuracy of the mesh.
|
static int |
_PERCENTAGE
Percentage option allows the user to reduce the facet count by overall percentage.
|
static int |
_SMALLEST_FACET
Smallest facet removes all facets smaller than the defined area, thus removing facets deemed to be redundant by the designer.
|
static DecimateFacetBodyBuilder.DecimateMethodType |
CHORDAL_DEVIATION
Chordal deviation reduces the number of facets by removing facets which do not effect the overall accuracy of the mesh.
|
static DecimateFacetBodyBuilder.DecimateMethodType |
PERCENTAGE
Percentage option allows the user to reduce the facet count by overall percentage.
|
static DecimateFacetBodyBuilder.DecimateMethodType |
SMALLEST_FACET
Smallest facet removes all facets smaller than the defined area, thus removing facets deemed to be redundant by the designer.
|
Modifier and Type | Method and Description |
---|---|
static DecimateFacetBodyBuilder.DecimateMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DecimateFacetBodyBuilder.DecimateMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DecimateFacetBodyBuilder.DecimateMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DecimateFacetBodyBuilder.DecimateMethodType CHORDAL_DEVIATION
public static final DecimateFacetBodyBuilder.DecimateMethodType SMALLEST_FACET
public static final DecimateFacetBodyBuilder.DecimateMethodType PERCENTAGE
public static final int _CHORDAL_DEVIATION
public static final int _SMALLEST_FACET
public static final int _PERCENTAGE
public static DecimateFacetBodyBuilder.DecimateMethodType valueOf(int value)
public static DecimateFacetBodyBuilder.DecimateMethodType valueOf(String name)
public static DecimateFacetBodyBuilder.DecimateMethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.