public static class StudioImageCaptureBuilder.DPIEnumType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DPI150
Set image at 150 DPI resolution
|
static int |
_DPI72
Set image at 72 DPI resolution
|
static StudioImageCaptureBuilder.DPIEnumType |
DPI150
Set image at 150 DPI resolution
|
static StudioImageCaptureBuilder.DPIEnumType |
DPI72
Set image at 72 DPI resolution
|
Modifier and Type | Method and Description |
---|---|
static StudioImageCaptureBuilder.DPIEnumType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioImageCaptureBuilder.DPIEnumType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioImageCaptureBuilder.DPIEnumType[] |
values()
Returns an array that contains the values for this enum.
|
public static final StudioImageCaptureBuilder.DPIEnumType DPI72
public static final StudioImageCaptureBuilder.DPIEnumType DPI150
public static final int _DPI72
public static final int _DPI150
public static StudioImageCaptureBuilder.DPIEnumType valueOf(int value)
public static StudioImageCaptureBuilder.DPIEnumType valueOf(String name)
public static StudioImageCaptureBuilder.DPIEnumType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.