public interface RasterImageBuilder extends ImageBaseBuilder
RasterImageBuilder
.
RasterImage
provides placing an imported image
onto a plane (with controls for orientation, sizing, and display) to use as
a reference in the model to create geometry.
ImageCollection.createRasterImageBuilder(nxopen.display.RasterImage)
Property | Value |
---|---|
BasePointChoice | BottomLeft |
ColorMode | Rgb |
InsertionPointOption | Default |
LockAspectRatio | 1 |
OverallTranslucency | 0 |
PixelColorTolerance | 32 |
ReferenceDirectionOption | Horizontal |
SizeOption | UserDefined |
TransparencyColorOption | None |
ImageBaseBuilder.BasePointChoices, ImageBaseBuilder.CornerPointsData, ImageBaseBuilder.ImageColorModes, ImageBaseBuilder.InsertionPoint, ImageBaseBuilder.ReferenceDirection, ImageBaseBuilder.SizeOptions, ImageBaseBuilder.TransparencyColorFrom
Modifier and Type | Method and Description |
---|---|
void |
setTarget(Plane targetObject)
License requirements: None. |
Plane |
target()
Returns the plane the raster image is placed onto
License requirements: None. |
alignImageToReferenceDirection, basePointChoice, colorMode, flipHorizontal, flipVertical, getBackgroundColor, getCornerPoints, getForegroundColor, getImagesInPart, getTransparentPixelColor, height, imageFile, imageReferencePoint1, imageReferencePoint2, imageReferencePoint3, insertionPointOption, lockAspectRatio, modelReferencePoint1, modelReferencePoint2, modelReferencePoint3, orientViewToImage, overallTranslucency, pixelColorTolerance, referenceDirectionOption, resetImageSize, rotateAngleOfReferenceVector, rotateLeft, rotateRight, setBackgroundColor, setBasePointChoice, setColorMode, setCornerPoints, setForegroundColor, setImageFile, setImageFromPart, setImageReferencePoint1, setImageReferencePoint2, setImageReferencePoint3, setInsertionPointOption, setLockAspectRatio, setModelReferencePoint1, setModelReferencePoint2, setModelReferencePoint3, setOverallTranslucency, setPixelColorTolerance, setReferenceDirectionOption, setSizeOption, setTransparencyColorOption, setTransparentPixelColor, setUserBasePoint, setUserInsertionPoint, setUserReferenceDirection, sizeOption, transparencyColorOption, userBasePoint, userInsertionPoint, userReferenceDirection, width
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
Plane target() throws NXException, RemoteException
NXException
RemoteException
void setTarget(Plane targetObject) throws NXException, RemoteException
targetObject
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.