public interface ImageCollection extends TaggedObjectCollection
BasePart
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
RasterImageBuilder |
createRasterImageBuilder(RasterImage image)
Creates a
RasterImageBuilder object
used to build an image. |
ImageBase |
findObject(String journalIdentifier)
Finds the
ImageBase with the given identifier
as recorded in a journal. |
_find_next, iterator
ImageBase findObject(String journalIdentifier) throws NXException, RemoteException
ImageBase
with the given identifier
as recorded in a journal. An object may not return the same value as
its JournalIdentifier in different versions of the software. However
newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In
general,this method should not be used in handwritten code and exists
to support record and playback of journals.
journalIdentifier
- Identifier to be foundNXException
RemoteException
RasterImageBuilder createRasterImageBuilder(RasterImage image) throws NXException, RemoteException
RasterImageBuilder
object
used to build an image.
If the image is not null, the image object will be edited.
image
- If image is not null,
this object will be editedNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.