public static class UncutRegionsBuilder.ResultsType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BOTH_SIDES
Find uncut regions on both sides of curve
|
static int |
_ONE_SIDE
Find uncut regions on one side only
|
static UncutRegionsBuilder.ResultsType |
BOTH_SIDES
Find uncut regions on both sides of curve
|
static UncutRegionsBuilder.ResultsType |
ONE_SIDE
Find uncut regions on one side only
|
Modifier and Type | Method and Description |
---|---|
static UncutRegionsBuilder.ResultsType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UncutRegionsBuilder.ResultsType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UncutRegionsBuilder.ResultsType[] |
values()
Returns an array that contains the values for this enum.
|
public static final UncutRegionsBuilder.ResultsType ONE_SIDE
public static final UncutRegionsBuilder.ResultsType BOTH_SIDES
public static final int _ONE_SIDE
public static final int _BOTH_SIDES
public static UncutRegionsBuilder.ResultsType valueOf(int value)
public static UncutRegionsBuilder.ResultsType valueOf(String name)
public static UncutRegionsBuilder.ResultsType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.