public static class HandlingCoreBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AT_LOCATION
Location specified by the user.
|
static int |
_FROM_BASE
Location is an offset from the base.
|
static int |
_MAP_FROM_BASE
Locate by finding the minimum distance to the main profile of the target and then project and offset from the base.
|
static HandlingCoreBuilder.Types |
AT_LOCATION
Location specified by the user.
|
static HandlingCoreBuilder.Types |
FROM_BASE
Location is an offset from the base.
|
static HandlingCoreBuilder.Types |
MAP_FROM_BASE
Locate by finding the minimum distance to the main profile of the target and then project and offset from the base.
|
Modifier and Type | Method and Description |
---|---|
static HandlingCoreBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HandlingCoreBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HandlingCoreBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final HandlingCoreBuilder.Types AT_LOCATION
public static final HandlingCoreBuilder.Types FROM_BASE
public static final HandlingCoreBuilder.Types MAP_FROM_BASE
public static final int _AT_LOCATION
public static final int _FROM_BASE
public static final int _MAP_FROM_BASE
public static HandlingCoreBuilder.Types valueOf(int value)
public static HandlingCoreBuilder.Types valueOf(String name)
public static HandlingCoreBuilder.Types[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.