public static class DrawBeadBuilder.TransitionDefinitionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
Shorten the bead segment that has the lowest height.
|
static int |
_MANUAL
User specified start and end segments so transition areas are fully defined.
|
static DrawBeadBuilder.TransitionDefinitionTypes |
AUTOMATIC
Shorten the bead segment that has the lowest height.
|
static DrawBeadBuilder.TransitionDefinitionTypes |
MANUAL
User specified start and end segments so transition areas are fully defined.
|
Modifier and Type | Method and Description |
---|---|
static DrawBeadBuilder.TransitionDefinitionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.TransitionDefinitionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.TransitionDefinitionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawBeadBuilder.TransitionDefinitionTypes AUTOMATIC
public static final DrawBeadBuilder.TransitionDefinitionTypes MANUAL
public static final int _AUTOMATIC
public static final int _MANUAL
public static DrawBeadBuilder.TransitionDefinitionTypes valueOf(int value)
public static DrawBeadBuilder.TransitionDefinitionTypes valueOf(String name)
public static DrawBeadBuilder.TransitionDefinitionTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.