public static class DrawBeadBuilder.OrientSectionToDrawTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DRAW_DIRECTION
Orient height parameter to the draw direction.
|
static int |
_SHEET_METAL_NORMAL
Orient height parameter to the sheet metal normal at the section location.
|
static DrawBeadBuilder.OrientSectionToDrawTypes |
DRAW_DIRECTION
Orient height parameter to the draw direction.
|
static DrawBeadBuilder.OrientSectionToDrawTypes |
SHEET_METAL_NORMAL
Orient height parameter to the sheet metal normal at the section location.
|
Modifier and Type | Method and Description |
---|---|
static DrawBeadBuilder.OrientSectionToDrawTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.OrientSectionToDrawTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.OrientSectionToDrawTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawBeadBuilder.OrientSectionToDrawTypes DRAW_DIRECTION
public static final DrawBeadBuilder.OrientSectionToDrawTypes SHEET_METAL_NORMAL
public static final int _DRAW_DIRECTION
public static final int _SHEET_METAL_NORMAL
public static DrawBeadBuilder.OrientSectionToDrawTypes valueOf(int value)
public static DrawBeadBuilder.OrientSectionToDrawTypes valueOf(String name)
public static DrawBeadBuilder.OrientSectionToDrawTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.