public class DiagrammingJumperprioritytype extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL
Horizontal
|
static int |
_VERTICAL
Vertical
|
static DiagrammingJumperprioritytype |
HORIZONTAL
Horizontal
|
static DiagrammingJumperprioritytype |
VERTICAL
Vertical
|
Modifier and Type | Method and Description |
---|---|
static DiagrammingJumperprioritytype |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DiagrammingJumperprioritytype |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DiagrammingJumperprioritytype[] |
values()
Returns an array that contains the values for this enum.
|
public static final DiagrammingJumperprioritytype HORIZONTAL
public static final DiagrammingJumperprioritytype VERTICAL
public static final int _HORIZONTAL
public static final int _VERTICAL
public static DiagrammingJumperprioritytype valueOf(int value)
public static DiagrammingJumperprioritytype valueOf(String name)
public static DiagrammingJumperprioritytype[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.