public static class TurnToolBuilder.ThicknessTypes extends Enum
Modifier and Type | Method and Description |
---|---|
static TurnToolBuilder.ThicknessTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnToolBuilder.ThicknessTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnToolBuilder.ThicknessTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnToolBuilder.ThicknessTypes THICKNESS01
public static final TurnToolBuilder.ThicknessTypes THICKNESS_T1
public static final TurnToolBuilder.ThicknessTypes THICKNESS02
public static final TurnToolBuilder.ThicknessTypes THICKNESS_T2
public static final TurnToolBuilder.ThicknessTypes THICKNESS03
public static final TurnToolBuilder.ThicknessTypes THICKNESS_T3
public static final TurnToolBuilder.ThicknessTypes THICKNESS04
public static final TurnToolBuilder.ThicknessTypes THICKNESS05
public static final TurnToolBuilder.ThicknessTypes THICKNESS06
public static final TurnToolBuilder.ThicknessTypes THICKNESS07
public static final TurnToolBuilder.ThicknessTypes THICKNESS09
public static final TurnToolBuilder.ThicknessTypes THICKNESS11
public static final TurnToolBuilder.ThicknessTypes THICKNESS12
public static final TurnToolBuilder.ThicknessTypes THICKNESS_USER_DEFINED
public static final int _THICKNESS01
public static final int _THICKNESS_T1
public static final int _THICKNESS02
public static final int _THICKNESS_T2
public static final int _THICKNESS03
public static final int _THICKNESS_T3
public static final int _THICKNESS04
public static final int _THICKNESS05
public static final int _THICKNESS06
public static final int _THICKNESS07
public static final int _THICKNESS09
public static final int _THICKNESS11
public static final int _THICKNESS12
public static final int _THICKNESS_USER_DEFINED
public static TurnToolBuilder.ThicknessTypes valueOf(int value)
public static TurnToolBuilder.ThicknessTypes valueOf(String name)
public static TurnToolBuilder.ThicknessTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.