public static class TurnAvoidanceClearanceBuilder.AxialPlaneModes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISTANCE
Plane is defined by distance value.
|
static int |
_NONE
Plane is inactive.
|
static int |
_POINT
Plane is defined by point.
|
static TurnAvoidanceClearanceBuilder.AxialPlaneModes |
DISTANCE
Plane is defined by distance value.
|
static TurnAvoidanceClearanceBuilder.AxialPlaneModes |
NONE
Plane is inactive.
|
static TurnAvoidanceClearanceBuilder.AxialPlaneModes |
POINT
Plane is defined by point.
|
Modifier and Type | Method and Description |
---|---|
static TurnAvoidanceClearanceBuilder.AxialPlaneModes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceClearanceBuilder.AxialPlaneModes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceClearanceBuilder.AxialPlaneModes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnAvoidanceClearanceBuilder.AxialPlaneModes NONE
public static final TurnAvoidanceClearanceBuilder.AxialPlaneModes POINT
public static final TurnAvoidanceClearanceBuilder.AxialPlaneModes DISTANCE
public static final int _NONE
public static final int _POINT
public static final int _DISTANCE
public static TurnAvoidanceClearanceBuilder.AxialPlaneModes valueOf(int value)
public static TurnAvoidanceClearanceBuilder.AxialPlaneModes valueOf(String name)
public static TurnAvoidanceClearanceBuilder.AxialPlaneModes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.