public static class TrimPoint.Options extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
Point is inactive.
|
static int |
_POINT
Point is active.
|
static TrimPoint.Options |
NONE
Point is inactive.
|
static TrimPoint.Options |
POINT
Point is active.
|
Modifier and Type | Method and Description |
---|---|
static TrimPoint.Options |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimPoint.Options |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimPoint.Options[] |
values()
Returns an array that contains the values for this enum.
|
public static final TrimPoint.Options NONE
public static final TrimPoint.Options POINT
public static final int _NONE
public static final int _POINT
public static TrimPoint.Options valueOf(int value)
public static TrimPoint.Options valueOf(String name)
public static TrimPoint.Options[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.