public static class TeachmodeProfileMoveBuilder.StartStopPositionMethods extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CHECK
Use selected check geometry
|
static int |
_CONTOUR_POSITION
Use end point of last contouring
|
static int |
_DRIVE
Use drive geometry start or stop point
|
static int |
_POINT
Use selected point
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
CHECK
Use selected check geometry
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
CONTOUR_POSITION
Use end point of last contouring
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
DRIVE
Use drive geometry start or stop point
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
POINT
Use selected point
|
Modifier and Type | Method and Description |
---|---|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods[] |
values()
Returns an array that contains the values for this enum.
|
public static final TeachmodeProfileMoveBuilder.StartStopPositionMethods DRIVE
public static final TeachmodeProfileMoveBuilder.StartStopPositionMethods POINT
public static final TeachmodeProfileMoveBuilder.StartStopPositionMethods CHECK
public static final TeachmodeProfileMoveBuilder.StartStopPositionMethods CONTOUR_POSITION
public static final int _DRIVE
public static final int _POINT
public static final int _CHECK
public static final int _CONTOUR_POSITION
public static TeachmodeProfileMoveBuilder.StartStopPositionMethods valueOf(int value)
public static TeachmodeProfileMoveBuilder.StartStopPositionMethods valueOf(String name)
public static TeachmodeProfileMoveBuilder.StartStopPositionMethods[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.