public static class IpwContainmentCurvesBuilder.ThicknessModeValue extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISTANCE
use thickness mode distance
|
static int |
_POINT
use thickness mode point
|
static IpwContainmentCurvesBuilder.ThicknessModeValue |
DISTANCE
use thickness mode distance
|
static IpwContainmentCurvesBuilder.ThicknessModeValue |
POINT
use thickness mode point
|
Modifier and Type | Method and Description |
---|---|
static IpwContainmentCurvesBuilder.ThicknessModeValue |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IpwContainmentCurvesBuilder.ThicknessModeValue |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IpwContainmentCurvesBuilder.ThicknessModeValue[] |
values()
Returns an array that contains the values for this enum.
|
public static final IpwContainmentCurvesBuilder.ThicknessModeValue POINT
public static final IpwContainmentCurvesBuilder.ThicknessModeValue DISTANCE
public static final int _POINT
public static final int _DISTANCE
public static IpwContainmentCurvesBuilder.ThicknessModeValue valueOf(int value)
public static IpwContainmentCurvesBuilder.ThicknessModeValue valueOf(String name)
public static IpwContainmentCurvesBuilder.ThicknessModeValue[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.