public static class InspectionToleranceOperationBuilder.TolType extends Enum
Modifier and Type | Method and Description |
---|---|
static InspectionToleranceOperationBuilder.TolType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionToleranceOperationBuilder.TolType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionToleranceOperationBuilder.TolType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionToleranceOperationBuilder.TolType DISTANCE_BETWEEN
public static final InspectionToleranceOperationBuilder.TolType ANGLE_BETWEEN
public static final InspectionToleranceOperationBuilder.TolType COORDINATE_TOLERANCE
public static final InspectionToleranceOperationBuilder.TolType DIAMETER
public static final InspectionToleranceOperationBuilder.TolType RADIUS
public static final InspectionToleranceOperationBuilder.TolType WIDTH
public static final InspectionToleranceOperationBuilder.TolType CONE_ANGLE
public static final InspectionToleranceOperationBuilder.TolType DATUM_DEFINITION
public static final InspectionToleranceOperationBuilder.TolType FLATNESS
public static final InspectionToleranceOperationBuilder.TolType STRAIGHTNESS
public static final InspectionToleranceOperationBuilder.TolType CIRCULARITY
public static final InspectionToleranceOperationBuilder.TolType CYLINDRICITY
public static final InspectionToleranceOperationBuilder.TolType LINE_PROFILE
public static final InspectionToleranceOperationBuilder.TolType SURFACE_PROFILE
public static final InspectionToleranceOperationBuilder.TolType ANGULARITY
public static final InspectionToleranceOperationBuilder.TolType PARALLELISM
public static final InspectionToleranceOperationBuilder.TolType PERPENDICULARITY
public static final InspectionToleranceOperationBuilder.TolType POSITION
public static final InspectionToleranceOperationBuilder.TolType CONCENTRICITY
public static final InspectionToleranceOperationBuilder.TolType SYMMETRY
public static final InspectionToleranceOperationBuilder.TolType CIRCULAR_RUNOUT
public static final InspectionToleranceOperationBuilder.TolType TOTAL_RUNOUT
public static final InspectionToleranceOperationBuilder.TolType DATUM_TARGET
public static final int _DISTANCE_BETWEEN
public static final int _ANGLE_BETWEEN
public static final int _COORDINATE_TOLERANCE
public static final int _DIAMETER
public static final int _RADIUS
public static final int _WIDTH
public static final int _CONE_ANGLE
public static final int _DATUM_DEFINITION
public static final int _FLATNESS
public static final int _STRAIGHTNESS
public static final int _CIRCULARITY
public static final int _CYLINDRICITY
public static final int _LINE_PROFILE
public static final int _SURFACE_PROFILE
public static final int _ANGULARITY
public static final int _PARALLELISM
public static final int _PERPENDICULARITY
public static final int _POSITION
public static final int _CONCENTRICITY
public static final int _SYMMETRY
public static final int _CIRCULAR_RUNOUT
public static final int _TOTAL_RUNOUT
public static final int _DATUM_TARGET
public static InspectionToleranceOperationBuilder.TolType valueOf(int value)
public static InspectionToleranceOperationBuilder.TolType valueOf(String name)
public static InspectionToleranceOperationBuilder.TolType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.