public static class InspectionSensorMassEditBuilder.SensorStrategyType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CREATEASNEEDED
Create as needed
|
static int |
_USEEXISTINGONLY
Use existing only
|
static InspectionSensorMassEditBuilder.SensorStrategyType |
CREATEASNEEDED
Create as needed
|
static InspectionSensorMassEditBuilder.SensorStrategyType |
USEEXISTINGONLY
Use existing only
|
Modifier and Type | Method and Description |
---|---|
static InspectionSensorMassEditBuilder.SensorStrategyType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionSensorMassEditBuilder.SensorStrategyType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionSensorMassEditBuilder.SensorStrategyType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionSensorMassEditBuilder.SensorStrategyType CREATEASNEEDED
public static final InspectionSensorMassEditBuilder.SensorStrategyType USEEXISTINGONLY
public static final int _CREATEASNEEDED
public static final int _USEEXISTINGONLY
public static InspectionSensorMassEditBuilder.SensorStrategyType valueOf(int value)
public static InspectionSensorMassEditBuilder.SensorStrategyType valueOf(String name)
public static InspectionSensorMassEditBuilder.SensorStrategyType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.