public static class InspectionOutputOperationBuilder.TypeOutput extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_OUTPUT1 |
static int |
_OUTPUT2 |
static InspectionOutputOperationBuilder.TypeOutput |
OUTPUT1 |
static InspectionOutputOperationBuilder.TypeOutput |
OUTPUT2 |
Modifier and Type | Method and Description |
---|---|
static InspectionOutputOperationBuilder.TypeOutput |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionOutputOperationBuilder.TypeOutput |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionOutputOperationBuilder.TypeOutput[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionOutputOperationBuilder.TypeOutput OUTPUT1
public static final InspectionOutputOperationBuilder.TypeOutput OUTPUT2
public static final int _OUTPUT1
public static final int _OUTPUT2
public static InspectionOutputOperationBuilder.TypeOutput valueOf(int value)
public static InspectionOutputOperationBuilder.TypeOutput valueOf(String name)
public static InspectionOutputOperationBuilder.TypeOutput[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.