public static class RSEvent.ResultFileType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DYNAMIC_RESPONSE
Result file to contain dynamic response evaluation results, which extension is ".rs2"
|
static int |
_FUNCTION_RESPONSE
Result file to contain function response evaluation results, which extenstion is ".afu"
|
static int |
_MODAL_RESPONSE
Result file to be used as Restart File, which extension is ".eef" or ".sef"
|
static RSEvent.ResultFileType |
DYNAMIC_RESPONSE
Result file to contain dynamic response evaluation results, which extension is ".rs2"
|
static RSEvent.ResultFileType |
FUNCTION_RESPONSE
Result file to contain function response evaluation results, which extenstion is ".afu"
|
static RSEvent.ResultFileType |
MODAL_RESPONSE
Result file to be used as Restart File, which extension is ".eef" or ".sef"
|
Modifier and Type | Method and Description |
---|---|
static RSEvent.ResultFileType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RSEvent.ResultFileType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RSEvent.ResultFileType[] |
values()
Returns an array that contains the values for this enum.
|
public static final RSEvent.ResultFileType MODAL_RESPONSE
public static final RSEvent.ResultFileType FUNCTION_RESPONSE
public static final RSEvent.ResultFileType DYNAMIC_RESPONSE
public static final int _MODAL_RESPONSE
public static final int _FUNCTION_RESPONSE
public static final int _DYNAMIC_RESPONSE
public static RSEvent.ResultFileType valueOf(int value)
public static RSEvent.ResultFileType valueOf(String name)
public static RSEvent.ResultFileType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.