public static class TBSTopologyRestrictAreaBuilder.CheckTypeOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CAST
Manufacturing restrictions to guarantee the manufacturing of the elements
|
static int |
_FROZEN
All elements of the element group which do not undergo any
changes during optimization
|
static int |
_LINK_TOPO
Definition of symmetry and link condtions
|
static int |
_MAXIMUMS_SIZE
Defition of the maximum structural diameter
|
static int |
_MINIMUM_SIZE
Definition of minimum structural diameter
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
CAST
Manufacturing restrictions to guarantee the manufacturing of the elements
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
FROZEN
All elements of the element group which do not undergo any
changes during optimization
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
LINK_TOPO
Definition of symmetry and link condtions
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
MAXIMUMS_SIZE
Defition of the maximum structural diameter
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
MINIMUM_SIZE
Definition of minimum structural diameter
|
Modifier and Type | Method and Description |
---|---|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSTopologyRestrictAreaBuilder.CheckTypeOption FROZEN
public static final TBSTopologyRestrictAreaBuilder.CheckTypeOption LINK_TOPO
public static final TBSTopologyRestrictAreaBuilder.CheckTypeOption MAXIMUMS_SIZE
public static final TBSTopologyRestrictAreaBuilder.CheckTypeOption MINIMUM_SIZE
public static final TBSTopologyRestrictAreaBuilder.CheckTypeOption CAST
public static final int _FROZEN
public static final int _LINK_TOPO
public static final int _MAXIMUMS_SIZE
public static final int _MINIMUM_SIZE
public static final int _CAST
public static TBSTopologyRestrictAreaBuilder.CheckTypeOption valueOf(int value)
public static TBSTopologyRestrictAreaBuilder.CheckTypeOption valueOf(String name)
public static TBSTopologyRestrictAreaBuilder.CheckTypeOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.