public interface SolidElementFaceNormalBuilder extends Builder, ISelectionBuilder
SolidElementFaceNormalBuilder
used to reorient normals
for left handed solid elements.
Both of the methods are only available in fem context.
ModelCheckManager.createSolidElementFaceNormalBuilder()
Modifier and Type | Method and Description |
---|---|
void |
createGroupOfLeftHandedElements()
Create group for the left handed elements in
createGroupOfLeftHandedElements()
and returns those elements which were grouped successfully. |
void |
displayNormals()
Display normals of
displayNormals()
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX11.0.0 |
int |
negativeFaceColor()
Returns the negative face color
License requirements: None. |
int |
positiveFaceColor()
Returns the positive face color
License requirements: None. |
void |
reorientLeftHandedElements()
Reorient normals specified in
reorientLeftHandedElements()
which normal is left handed and returns those elements whose normals were reoriented successfully. |
SelectTaggedObjectList |
selectionList()
Returns the selected objects to be checked.
|
void |
setNegativeFaceColor(int negativeFaceColor)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setPositiveFaceColor(int positiveFaceColor)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
checkScopeOption, setCheckScopeOption
SelectTaggedObjectList selectionList() throws NXException, RemoteException
Mesh
or
FEElement
NXException
RemoteException
void displayNormals() throws NXException, RemoteException
displayNormals()
NXException
RemoteException
void reorientLeftHandedElements() throws NXException, RemoteException
reorientLeftHandedElements()
which normal is left handed and returns those elements whose normals were reoriented successfully. This method will only reorient
the normals for solid left handed elements in the current work fem part.
NXException
RemoteException
void createGroupOfLeftHandedElements() throws NXException, RemoteException
createGroupOfLeftHandedElements()
and returns those elements which were grouped successfully. This method will only group left handed solid elements
in the current work fem part.
NXException
RemoteException
int positiveFaceColor() throws NXException, RemoteException
NXException
RemoteException
void setPositiveFaceColor(int positiveFaceColor) throws NXException, RemoteException
positiveFaceColor
- NXException
RemoteException
int negativeFaceColor() throws NXException, RemoteException
NXException
RemoteException
void setNegativeFaceColor(int negativeFaceColor) throws NXException, RemoteException
negativeFaceColor
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.