public interface ReverseBeamElementDirectionBuilder extends Builder, ISelectionBuilder
ReverseBeamElementDirectionBuilder
used to reverse directions
for specified beam elements. You can reverse beam element directions by using either Builder.commit()
or reverseDirections()
.
The difference between these two methods is Builder.commit()
reverses the directions
and updates direction display, but it does not return the beam elements which were reversed
successfully. reverseDirections()
reverses directions and returns the beam elements which were reversed successfully.
Both of the methods are only available in fem context.
ModelCheckManager.createReverseBeamElementDirectionBuilder()
Modifier and Type | Method and Description |
---|---|
void |
displayDirections()
Display directions of
selectionList()
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.5.0 |
FEElement[] |
reverseDirections()
Reverses directions specified in
selectionList()
and returns those elements whose directions were reversed successfully. |
SelectTaggedObjectList |
selectionList()
Returns the selected objects to be checked.
|
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
checkScopeOption, setCheckScopeOption
SelectTaggedObjectList selectionList() throws NXException, RemoteException
Mesh
or
FEElement
NXException
RemoteException
void displayDirections() throws NXException, RemoteException
selectionList()
NXException
RemoteException
FEElement[] reverseDirections() throws NXException, RemoteException
selectionList()
and returns those elements whose directions were reversed successfully. This method will only reverse
the directions for beam elements in the current work fem part.
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.