public static class InputLoad.LoadSupportType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ELEMENT
Element (the method has to aggregated values that have been extracted per element, GetValues() will return a table of values)
|
static int |
_NODE
Node (the method has to aggregated values that have been extracted per node, GetValues() will return a table of values)
|
static int |
_NONE
not available (the aggregation has been done at the calculation level, GetValues() will return a vector of aggregated values)
|
static InputLoad.LoadSupportType |
ELEMENT
Element (the method has to aggregated values that have been extracted per element, GetValues() will return a table of values)
|
static InputLoad.LoadSupportType |
NODE
Node (the method has to aggregated values that have been extracted per node, GetValues() will return a table of values)
|
static InputLoad.LoadSupportType |
NONE
not available (the aggregation has been done at the calculation level, GetValues() will return a vector of aggregated values)
|
Modifier and Type | Method and Description |
---|---|
static InputLoad.LoadSupportType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InputLoad.LoadSupportType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InputLoad.LoadSupportType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InputLoad.LoadSupportType NONE
public static final InputLoad.LoadSupportType NODE
public static final InputLoad.LoadSupportType ELEMENT
public static final int _NONE
public static final int _NODE
public static final int _ELEMENT
public static InputLoad.LoadSupportType valueOf(int value)
public static InputLoad.LoadSupportType valueOf(String name)
public static InputLoad.LoadSupportType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.