public static class SolidPropertyCheckBuilder.UserUnit extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFAULT_UNIT
Load unit = same as system default unit
|
static int |
_KG_MILLI
mass = kg, cg = mm, volume = mm^3 mmoi = kg-mm^2
|
static int |
_LBF_IN_SEC
mass = lbf-sec^2/in, cg = in, volume = in^3 mmoi = lbf-in-sec^2
|
static int |
_LBM_IN
mass = lbm, cg = in, volume = in^3 mmoi = lbm-in^2
|
static SolidPropertyCheckBuilder.UserUnit |
DEFAULT_UNIT
Load unit = same as system default unit
|
static SolidPropertyCheckBuilder.UserUnit |
KG_MILLI
mass = kg, cg = mm, volume = mm^3 mmoi = kg-mm^2
|
static SolidPropertyCheckBuilder.UserUnit |
LBF_IN_SEC
mass = lbf-sec^2/in, cg = in, volume = in^3 mmoi = lbf-in-sec^2
|
static SolidPropertyCheckBuilder.UserUnit |
LBM_IN
mass = lbm, cg = in, volume = in^3 mmoi = lbm-in^2
|
Modifier and Type | Method and Description |
---|---|
static SolidPropertyCheckBuilder.UserUnit |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SolidPropertyCheckBuilder.UserUnit |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SolidPropertyCheckBuilder.UserUnit[] |
values()
Returns an array that contains the values for this enum.
|
public static final SolidPropertyCheckBuilder.UserUnit DEFAULT_UNIT
public static final SolidPropertyCheckBuilder.UserUnit KG_MILLI
public static final SolidPropertyCheckBuilder.UserUnit LBM_IN
public static final SolidPropertyCheckBuilder.UserUnit LBF_IN_SEC
public static final int _DEFAULT_UNIT
public static final int _KG_MILLI
public static final int _LBM_IN
public static final int _LBF_IN_SEC
public static SolidPropertyCheckBuilder.UserUnit valueOf(int value)
public static SolidPropertyCheckBuilder.UserUnit valueOf(String name)
public static SolidPropertyCheckBuilder.UserUnit[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.