public static class QueryCurveUsageOptions.ResultantCurveLocatorType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SNAP_TO_CLOSEST_NODE |
static int |
_USE_AS_IS |
static int |
_USE_INTERSECTED_ELEMENTS |
static QueryCurveUsageOptions.ResultantCurveLocatorType |
SNAP_TO_CLOSEST_NODE |
static QueryCurveUsageOptions.ResultantCurveLocatorType |
USE_AS_IS |
static QueryCurveUsageOptions.ResultantCurveLocatorType |
USE_INTERSECTED_ELEMENTS |
Modifier and Type | Method and Description |
---|---|
static QueryCurveUsageOptions.ResultantCurveLocatorType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static QueryCurveUsageOptions.ResultantCurveLocatorType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static QueryCurveUsageOptions.ResultantCurveLocatorType[] |
values()
Returns an array that contains the values for this enum.
|
public static final QueryCurveUsageOptions.ResultantCurveLocatorType USE_AS_IS
public static final QueryCurveUsageOptions.ResultantCurveLocatorType SNAP_TO_CLOSEST_NODE
public static final QueryCurveUsageOptions.ResultantCurveLocatorType USE_INTERSECTED_ELEMENTS
public static final int _USE_AS_IS
public static final int _SNAP_TO_CLOSEST_NODE
public static final int _USE_INTERSECTED_ELEMENTS
public static QueryCurveUsageOptions.ResultantCurveLocatorType valueOf(int value)
public static QueryCurveUsageOptions.ResultantCurveLocatorType valueOf(String name)
public static QueryCurveUsageOptions.ResultantCurveLocatorType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.