public static class NumberFormat.FormatOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
The program will determine the format internally
|
static int |
_FIXED
Format the number in fixed decimals
|
static int |
_SCIENTIFIC
Format the number in scientific
|
static NumberFormat.FormatOption |
AUTOMATIC
The program will determine the format internally
|
static NumberFormat.FormatOption |
FIXED
Format the number in fixed decimals
|
static NumberFormat.FormatOption |
SCIENTIFIC
Format the number in scientific
|
Modifier and Type | Method and Description |
---|---|
static NumberFormat.FormatOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NumberFormat.FormatOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NumberFormat.FormatOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final NumberFormat.FormatOption AUTOMATIC
public static final NumberFormat.FormatOption FIXED
public static final NumberFormat.FormatOption SCIENTIFIC
public static final int _AUTOMATIC
public static final int _FIXED
public static final int _SCIENTIFIC
public static NumberFormat.FormatOption valueOf(int value)
public static NumberFormat.FormatOption valueOf(String name)
public static NumberFormat.FormatOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.