public static class NodesBetweenNodesBuilder.TypeEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NODE_AT_CENTER_OF_THREE_NODES
At the center of imaginary circle defined by 3 nodes
|
static int |
_NODES_BETWEEN_TWO_NODES
Between two nodes
|
static NodesBetweenNodesBuilder.TypeEnum |
NODE_AT_CENTER_OF_THREE_NODES
At the center of imaginary circle defined by 3 nodes
|
static NodesBetweenNodesBuilder.TypeEnum |
NODES_BETWEEN_TWO_NODES
Between two nodes
|
Modifier and Type | Method and Description |
---|---|
static NodesBetweenNodesBuilder.TypeEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NodesBetweenNodesBuilder.TypeEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NodesBetweenNodesBuilder.TypeEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final NodesBetweenNodesBuilder.TypeEnum NODES_BETWEEN_TWO_NODES
public static final NodesBetweenNodesBuilder.TypeEnum NODE_AT_CENTER_OF_THREE_NODES
public static final int _NODES_BETWEEN_TWO_NODES
public static final int _NODE_AT_CENTER_OF_THREE_NODES
public static NodesBetweenNodesBuilder.TypeEnum valueOf(int value)
public static NodesBetweenNodesBuilder.TypeEnum valueOf(String name)
public static NodesBetweenNodesBuilder.TypeEnum[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.