public static class ModelUpdateCorrelMethodBuilder.Method extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAC
Correlation Method is MAC
|
static int |
_XORTHO
Correlation Method is X_ORTHO
|
static ModelUpdateCorrelMethodBuilder.Method |
MAC
Correlation Method is MAC
|
static ModelUpdateCorrelMethodBuilder.Method |
XORTHO
Correlation Method is X_ORTHO
|
Modifier and Type | Method and Description |
---|---|
static ModelUpdateCorrelMethodBuilder.Method |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelUpdateCorrelMethodBuilder.Method |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelUpdateCorrelMethodBuilder.Method[] |
values()
Returns an array that contains the values for this enum.
|
public static final ModelUpdateCorrelMethodBuilder.Method MAC
public static final ModelUpdateCorrelMethodBuilder.Method XORTHO
public static final int _MAC
public static final int _XORTHO
public static ModelUpdateCorrelMethodBuilder.Method valueOf(int value)
public static ModelUpdateCorrelMethodBuilder.Method valueOf(String name)
public static ModelUpdateCorrelMethodBuilder.Method[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.