public static class LaminateQuickReportBuilder.EnvelopeRule extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ABS_MAX
Keep maximum absolute values
|
static int |
_ABS_MIN
Keep minimum absolute values
|
static int |
_MAX
Keep maximum values
|
static int |
_MAX_MIN
Keep minimum and maximum values
|
static int |
_MIN
Keep minimum values
|
static LaminateQuickReportBuilder.EnvelopeRule |
ABS_MAX
Keep maximum absolute values
|
static LaminateQuickReportBuilder.EnvelopeRule |
ABS_MIN
Keep minimum absolute values
|
static LaminateQuickReportBuilder.EnvelopeRule |
MAX
Keep maximum values
|
static LaminateQuickReportBuilder.EnvelopeRule |
MAX_MIN
Keep minimum and maximum values
|
static LaminateQuickReportBuilder.EnvelopeRule |
MIN
Keep minimum values
|
Modifier and Type | Method and Description |
---|---|
static LaminateQuickReportBuilder.EnvelopeRule |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaminateQuickReportBuilder.EnvelopeRule |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaminateQuickReportBuilder.EnvelopeRule[] |
values()
Returns an array that contains the values for this enum.
|
public static final LaminateQuickReportBuilder.EnvelopeRule MAX_MIN
public static final LaminateQuickReportBuilder.EnvelopeRule MIN
public static final LaminateQuickReportBuilder.EnvelopeRule MAX
public static final LaminateQuickReportBuilder.EnvelopeRule ABS_MAX
public static final LaminateQuickReportBuilder.EnvelopeRule ABS_MIN
public static final int _MAX_MIN
public static final int _MIN
public static final int _MAX
public static final int _ABS_MAX
public static final int _ABS_MIN
public static LaminateQuickReportBuilder.EnvelopeRule valueOf(int value)
public static LaminateQuickReportBuilder.EnvelopeRule valueOf(String name)
public static LaminateQuickReportBuilder.EnvelopeRule[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.