public interface FrfSetBuilder extends AlternateFemRepresentationSourceBuilder
Modifier and Type | Method and Description |
---|---|
void |
deselectFrfsubsets(String[] frfSubSetNames)
Deselect the frf subset that should not be used.
|
String[] |
getAvailableFrfsubsets()
Get the frf subsets available in the source file of the
FrfSet
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX12.0.0 |
commitAlternateFemRepresentationSource, setFilePath, setLengthUnit, setMassUnit, setMeshCreationMode, setName, setResultReference
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
String[] getAvailableFrfsubsets() throws NXException, RemoteException
FrfSet
NXException
RemoteException
void deselectFrfsubsets(String[] frfSubSetNames) throws NXException, RemoteException
getAvailableFrfsubsets()
.
Should be called if getAvailableFrfsubsets()
returns several frf subsets.
If this method is not called, all frf subsets are supposed to be selected.
frfSubSetNames
- The frf subsets.NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.