public static class ElementAssociatedDataUtils.AskSpringData extends Object implements Serializable
ElementAssociatedDataUtils.askSpringData(nxopen.cae.FEElement)
Modifier and Type | Field and Description |
---|---|
CaeElementAssociatedDataUtilsComponentEnd |
componentenda
Component end A of the spring element (either translational or rotational).
|
CaeElementAssociatedDataUtilsComponentEnd |
componentendb
Component end B of the spring element (either translational or rotational).
|
boolean |
hasassociateddatadefined
True if element has element associated data defined.
|
PhysicalPropertyTable |
physicalpropertytable
Physical property table of the spring element.
|
double |
stiffness
Spring stiffness value either translational in units N/mm or lbf/in
or rotational in units N-mm or lbf-in.
|
Constructor and Description |
---|
AskSpringData() |
public boolean hasassociateddatadefined
public PhysicalPropertyTable physicalpropertytable
public double stiffness
public CaeElementAssociatedDataUtilsComponentEnd componentenda
public CaeElementAssociatedDataUtilsComponentEnd componentendb
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.