public static class ElementAssociatedDataUtils.AskDamperData extends Object implements Serializable
ElementAssociatedDataUtils.askDamperData(nxopen.cae.FEElement)
Modifier and Type | Field and Description |
---|---|
CaeElementAssociatedDataUtilsComponentEnd |
componentenda
Component end A of the damper element (either translational or rotational).
|
CaeElementAssociatedDataUtilsComponentEnd |
componentendb
Component end B of the damper element (either translational or rotational).
|
boolean |
hasassociateddatadefined
True if element has element associated data defined.
|
PhysicalPropertyTable |
physicalpropertytable
Physical property table of the damper element.
|
double |
viscousdamping
Viscous damping value either translational in units N-sec/mm or lbf-sec/in
or rotational in units mN-mm-sec or lbf-in-sec.
|
Constructor and Description |
---|
AskDamperData() |
public boolean hasassociateddatadefined
public double viscousdamping
public PhysicalPropertyTable physicalpropertytable
public CaeElementAssociatedDataUtilsComponentEnd componentenda
public CaeElementAssociatedDataUtilsComponentEnd componentendb
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.