public static class DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CRITICAL_PLANE
Critical Plane
|
static int |
_MAXIMUM_DAMAGE
Maximum Damage
|
static int |
_PRINCIPAL_AXIS
Principal Axis
|
static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum |
CRITICAL_PLANE
Critical Plane
|
static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum |
MAXIMUM_DAMAGE
Maximum Damage
|
static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum |
PRINCIPAL_AXIS
Principal Axis
|
Modifier and Type | Method and Description |
---|---|
static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum CRITICAL_PLANE
public static final DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum MAXIMUM_DAMAGE
public static final DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum PRINCIPAL_AXIS
public static final int _CRITICAL_PLANE
public static final int _MAXIMUM_DAMAGE
public static final int _PRINCIPAL_AXIS
public static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum valueOf(int value)
public static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum valueOf(String name)
public static DurabilityStressAxesBuilder.StressAxisDirectionSearchMethodEnum[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.