public static class DurSpecialistSolutionBuilder.MaterialSourceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INHERIT_FROM_SIMULATION
The material from the SIM/FEM document
|
static int |
_MATERIAL_LIBRARY
The material from the material library
|
static DurSpecialistSolutionBuilder.MaterialSourceType |
INHERIT_FROM_SIMULATION
The material from the SIM/FEM document
|
static DurSpecialistSolutionBuilder.MaterialSourceType |
MATERIAL_LIBRARY
The material from the material library
|
Modifier and Type | Method and Description |
---|---|
static DurSpecialistSolutionBuilder.MaterialSourceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurSpecialistSolutionBuilder.MaterialSourceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurSpecialistSolutionBuilder.MaterialSourceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DurSpecialistSolutionBuilder.MaterialSourceType INHERIT_FROM_SIMULATION
public static final DurSpecialistSolutionBuilder.MaterialSourceType MATERIAL_LIBRARY
public static final int _INHERIT_FROM_SIMULATION
public static final int _MATERIAL_LIBRARY
public static DurSpecialistSolutionBuilder.MaterialSourceType valueOf(int value)
public static DurSpecialistSolutionBuilder.MaterialSourceType valueOf(String name)
public static DurSpecialistSolutionBuilder.MaterialSourceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.