public static class AxiSymmetricParameters.EnvVal extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ABSOLUTE_MAXIMUM |
static int |
_ABSOLUTE_MINIMUM |
static int |
_AVERAGE |
static int |
_MAXIMUM |
static int |
_MINIMUM |
static int |
_SUM |
static AxiSymmetricParameters.EnvVal |
ABSOLUTE_MAXIMUM |
static AxiSymmetricParameters.EnvVal |
ABSOLUTE_MINIMUM |
static AxiSymmetricParameters.EnvVal |
AVERAGE |
static AxiSymmetricParameters.EnvVal |
MAXIMUM |
static AxiSymmetricParameters.EnvVal |
MINIMUM |
static AxiSymmetricParameters.EnvVal |
SUM |
Modifier and Type | Method and Description |
---|---|
static AxiSymmetricParameters.EnvVal |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AxiSymmetricParameters.EnvVal |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AxiSymmetricParameters.EnvVal[] |
values()
Returns an array that contains the values for this enum.
|
public static final AxiSymmetricParameters.EnvVal MAXIMUM
public static final AxiSymmetricParameters.EnvVal MINIMUM
public static final AxiSymmetricParameters.EnvVal ABSOLUTE_MAXIMUM
public static final AxiSymmetricParameters.EnvVal ABSOLUTE_MINIMUM
public static final AxiSymmetricParameters.EnvVal AVERAGE
public static final AxiSymmetricParameters.EnvVal SUM
public static final int _MAXIMUM
public static final int _MINIMUM
public static final int _ABSOLUTE_MAXIMUM
public static final int _ABSOLUTE_MINIMUM
public static final int _AVERAGE
public static final int _SUM
public static AxiSymmetricParameters.EnvVal valueOf(int value)
public static AxiSymmetricParameters.EnvVal valueOf(String name)
public static AxiSymmetricParameters.EnvVal[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.