public interface AutoCyclicSymmetryPairsBuilder extends Builder
AutoPairs
object which represents
a recipe for generating face pairs from a selected set of faces in the
model. Faces are selected as a pair if they are the same face (within an
angle and distance tolerance) when rotated about an axis. Pairs are only found
on the same body(ies) as the face(s) specified. This builder should only be used
for the creation of new Cyclic Symmetry BCs.
SimSimulation.createAutoCyclicSymmetryPairsBuilder(java.lang.String)
Modifier and Type | Method and Description |
---|---|
SelectCAEFaceList |
geometrySelection()
Returns the geometry selection
License requirements: None. |
void |
previewButton()
Preview the list of face-pairs
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
PropertyTable |
propertyTable()
Returns the AutoPair's property table
License requirements: None. |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectCAEFaceList geometrySelection() throws NXException, RemoteException
NXException
RemoteException
PropertyTable propertyTable() throws NXException, RemoteException
NXException
RemoteException
void previewButton() throws NXException, RemoteException
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.