public static class AssignNodalCSBuilder.GeometryOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BOUNDARY_NODES_ONLY
boundary nodes only
|
static int |
_INTERIOR_NODES_ONLY
interior nodes only
|
static int |
_INTERIORAND_BOUNDARY_NODES
interior and boundary
|
static AssignNodalCSBuilder.GeometryOption |
BOUNDARY_NODES_ONLY
boundary nodes only
|
static AssignNodalCSBuilder.GeometryOption |
INTERIOR_NODES_ONLY
interior nodes only
|
static AssignNodalCSBuilder.GeometryOption |
INTERIORAND_BOUNDARY_NODES
interior and boundary
|
Modifier and Type | Method and Description |
---|---|
static AssignNodalCSBuilder.GeometryOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssignNodalCSBuilder.GeometryOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssignNodalCSBuilder.GeometryOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final AssignNodalCSBuilder.GeometryOption INTERIOR_NODES_ONLY
public static final AssignNodalCSBuilder.GeometryOption BOUNDARY_NODES_ONLY
public static final AssignNodalCSBuilder.GeometryOption INTERIORAND_BOUNDARY_NODES
public static final int _INTERIOR_NODES_ONLY
public static final int _BOUNDARY_NODES_ONLY
public static final int _INTERIORAND_BOUNDARY_NODES
public static AssignNodalCSBuilder.GeometryOption valueOf(int value)
public static AssignNodalCSBuilder.GeometryOption valueOf(String name)
public static AssignNodalCSBuilder.GeometryOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.