public static class OnestepUnformBuilder.Constraint extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CURVE_ALONG_CURVE
Curve along Curve Constraint, used for complete unform only
|
static int |
_CURVE_TO_CURVE
Curve to Curve Constraint, used for intermediate unform only
|
static int |
_POINT_TO_POINT
Point to Point Constraint, used for complete unform only
|
static OnestepUnformBuilder.Constraint |
CURVE_ALONG_CURVE
Curve along Curve Constraint, used for complete unform only
|
static OnestepUnformBuilder.Constraint |
CURVE_TO_CURVE
Curve to Curve Constraint, used for intermediate unform only
|
static OnestepUnformBuilder.Constraint |
POINT_TO_POINT
Point to Point Constraint, used for complete unform only
|
Modifier and Type | Method and Description |
---|---|
static OnestepUnformBuilder.Constraint |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OnestepUnformBuilder.Constraint |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OnestepUnformBuilder.Constraint[] |
values()
Returns an array that contains the values for this enum.
|
public static final OnestepUnformBuilder.Constraint CURVE_TO_CURVE
public static final OnestepUnformBuilder.Constraint POINT_TO_POINT
public static final OnestepUnformBuilder.Constraint CURVE_ALONG_CURVE
public static final int _CURVE_TO_CURVE
public static final int _POINT_TO_POINT
public static final int _CURVE_ALONG_CURVE
public static OnestepUnformBuilder.Constraint valueOf(int value)
public static OnestepUnformBuilder.Constraint valueOf(String name)
public static OnestepUnformBuilder.Constraint[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.