Package | Description |
---|---|
nxopen.blockstyler |
Provides classes and interfaces for Block Styler.
|
Modifier and Type | Field and Description |
---|---|
static Tree.ControlType |
Tree.ControlType.COMBO_BOX
Combo box.
|
static Tree.ControlType |
Tree.ControlType.LIST_BOX
List box.
|
static Tree.ControlType |
Tree.ControlType.NONE
None
|
Modifier and Type | Method and Description |
---|---|
Tree.ControlType |
Tree.AskEditControlCallback.askEditControlCallback(Tree tree,
Node node,
int columnID)
Represents the callback which gets called when edit is attempted on any cell.
|
static Tree.ControlType |
Tree.ControlType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Tree.ControlType |
Tree.ControlType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Tree.ControlType[] |
Tree.ControlType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
Tree.EditControlOption |
Tree.OnEditOptionSelectedCallback.onEditOptionSelectedCallback(Tree tree,
Node node,
int columnID,
int selectedOptionID,
String selectedOptionText,
Tree.ControlType type)
Represents the callback which gets called when user selects an option in edit-control set by
BlockStyler.Tree.AskEditControlCallback.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.