public static class BlockDialog.DialogMode extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CREATE
When the user presses Ok or Apply on the
dialog, the user's inputs are saved in dialog memory and the next time that the dialog
is shown in Create mode, the dialog is initialized using the user's previous
inputs.
|
static int |
_EDIT
The Apply button is not shown.
|
static BlockDialog.DialogMode |
CREATE
When the user presses Ok or Apply on the
dialog, the user's inputs are saved in dialog memory and the next time that the dialog
is shown in Create mode, the dialog is initialized using the user's previous
inputs.
|
static BlockDialog.DialogMode |
EDIT
The Apply button is not shown.
|
Modifier and Type | Method and Description |
---|---|
static BlockDialog.DialogMode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlockDialog.DialogMode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlockDialog.DialogMode[] |
values()
Returns an array that contains the values for this enum.
|
public static final BlockDialog.DialogMode CREATE
public static final BlockDialog.DialogMode EDIT
public static final int _CREATE
public static final int _EDIT
public static BlockDialog.DialogMode valueOf(int value)
public static BlockDialog.DialogMode valueOf(String name)
public static BlockDialog.DialogMode[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.